Hard disk drives are today's fastest permanent storage media and have a large capacity. For this two reasons they are the most used storage medium in computers and servers. When buying a new hard disk, there are three important things to consider: - The connection of the disk to the computer or other device you will be using it with has a big influence on the speed with which data can be read from/written to the disk. Make sure the connection of the disk you buy is compatible with your computer! - The rotational speed is also important for the speed with which data can be read from/written to the disk and determines the time it takes to find a file on the disk. - Last but not least, the storage capacity of the disk, i.e. the amount of data that can be stored on the disk.
Release date: 15 May 2007
Info modified on: 03 Jun 2009 10:30:11
Product views: 22930
This statistic is based on the
6815
using ecommerce sites (eshops, distributors, comparison sites, ecommerce ASPs, purchase systems, etc) downloading this ICEcat data-sheet since
15 May 2007.
Only sponsoring brands are included in the free Open ICEcat content distribution as used by
6324
free Open ICEcat users .
Hard disk drives are today's fastest permanent storage media and have a large capacity. For this two reasons they are the most used storage medium in computers and servers. When buying a new hard disk, there are three important things to consider: - The connection of the disk to the computer or other device you will be using it with has a big influence on the speed with which data can be read from/written to the disk. Make sure the connection of the disk you buy is compatible with your computer! - The rotational speed is also important for the speed with which data can be read from/written to the disk and determines the time it takes to find a file on the disk. - Last but not least, the storage capacity of the disk, i.e. the amount of data that can be stored on the disk.
- 4200 rpm high-speed performance - Bus-powered (requires 2 USB ports) - Compact and lightweight - Fanless design for near-silent operation
Specs
Alternatives
Options
Disk drive
Hard disk drive capacity
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).
200 GB
Internal
The device is built in, or needs to be built in (Yes/No). No, means that the device is connected externally via wire or wireless.
Hard disk rotational speed
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
4200 RPM
Hard disk interface
USB 2.0
Hard disk size
2.5 "
Average latency
The average duration before a device can start with a job (for example reading a file from a hard disk).
12 ms
Track to track seek time (read/write)
2.0 ms
Drive device, buffer size
8 MB
Data transmission
Drive device, transfer rate
480 MB/s
Data transfer rate (max)
The maximum speed with which data can be transmitted from one device to another.
1200 Mbit/s
Connectivity
I/O ports
An interface on a device to which you can connect another device.
high-speed USB 2.0
Operating system/software
Compatible operating systems
List of desktop operating systems tested as compatible with this product, including coined name and version
Windows 2000/XP/Vista
Weight & dimensions
Weight
Weight of the product without packaging (nett weight). If possible, the nett weight is given including standard accessories and supplies. Please, note that sometimes the manufacturer is giving a too commercial interpretation of product weight, by leaving out the weight of accessories and/or supplies.