IceCat.biz cool in catalogues.
Search
 Netherlands Germany Spain United States Belgium Italy France Denmark UnitedKingdom Sweden Finland Austria Switzerland China Ukraine India Russian Federation Georgia Poland Portugal  More >> Country Language: English

Start > notebooks/laptops > Toshiba PSLE0E-006004BT

Satellite L350D-105

Brand: Toshiba
Product code: PSLE0E-006004BT
EAN/UPC code: 4026203557826
Product family: Satellite
Category: notebooks/laptops 
A notebook, also known as laptop, is a portable computer. When you are looking for the right notebook, it is important to know where you are going to work with it. Do you want to use it on the road? Choose a model with a special energy saving 'mobile' processor, a good battery and a reasonably small display. This will allow you to work longer with the same battery and saves you the trouble of carrying around a large display that consumes a lot of precious battery power. Or will you be using you notebook mainly in places where you will have access to a power outlet? Then choose a desktop processor (more processing power for less money) and an ordinary battery, this will save you a lot of money, which you could spend on a bigger screen, you'll work faster because you can view more information at once and it's great for multimedia!
Release date: 12 Mar 2008
Info modified on: 03 Jun 2009 10:30:11
PSLE0E-006004BT Toshiba
11k

Specs
Alternatives
Options
Processor
Processor clock speed
Processor speed in Mhz. Often the clock speed is expressed by a manufacturer in GHz (1 GHz = 1000 MHz). The clock rate is the fundamental rate in cycles per second (measured in hertz) at which a computer performs its most basic operations such as adding two numbers. There are more factors, like internal memory size, that influence a computer's actual response time.
1900 MHz
Processor family
The processor serie to which the processor belongs.
AMD Athlon
Processor
Processor is the central unit in a computer containing the logic circuitry that performs the instructions of a computer's programs.
AMD Athlon 64 X2 Dual-Core TK-57
Processor front side bus
Speed of the processor's Front Side Bus (FSB) in megahertz (1 million Herz). The FSB is the bus that transfers data between the CPU and the northbridge of the Motherboard. The maximum theoretical bandwidth of the FSB is determined by the product of its width, its clock frequency and the number of data transfers it performs per clock tick.
800 MHz
Chipset
Chipset for this configuration; expressed as manufacturer and coined name
AMD M690V
L2 cache
The CPU cache (Level 2 in megabyte) is a smaller, faster memory which stores copies of the data from the most frequently used main memory locations.
0.512 MB
Disk drive
Total storage capacity
Total storage capacity in Gigabyte (1 billion bytes).
120 GB
Hard disk interface SATA
Hard disk rotational speed
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
5400 RPM
Display
Display diagonal
Size of the display for this product; expressed in inches diagonal
17 "
Display
The display technology. Flat screen technologies like Liquid Cristal Display (LCD) and Thin Film Transistor (TFT) active matrix technology are the trend. In TV technologies one can notice FST (Flat Screen Tube) technology, and ARASC (Anti Reflexion, Anti Static Coating) or AGARAS (Anti-Glare ARASC) or simply AGC (anti-glare coating). The old tv and screen technology CRT means Cathodic Ray Tube. MLA = Micro Lens Array. p-Si=Polycrystalline Silicon. a-Si=Amorphous Silicon.
TruBrite® WXGA+ TFT
Display resolution
Resolution of the display for the system
1440 x 900 pixels
Aspect ratio 16:10
Memory
Internal memory
The amount of memory measured in megabytes installed in the system's hardware
2048 MB
Internal memory type DDR2
Memory layout
Describe how memory is plugged on the motherboard
2 x 1024 MB
Maximum internal memory 4 GB
Memory clock speed 667 MHz
Video
Graphic adapter ATI Radeon X1200
Maximum graphic adapter memory
Graphics memory is determining with the (graphic) processor, the graphics/video performance of your computer. Graphics memory is often shared with system memory so that it varies depending on the amount of system memory installed and system load.
831 MB
Graphics adapter manufacturer ATI
Optical drive
Optical drive type
Type of the optical drive
DVD Super Multi (DL)
DVD+R Double Layer read speed 8 x
DVD+R Double Layer write speed 4 x
DVD-R Dual Layer read speed 8 x
DVD-R Double Layer write speed 4 x
DVD-RAM read speed 5 x
DVD-RAM write speed 5 x
DVD+R read speed 8 x
DVD+R write speed 8 x
DVD-R write speed 8 x
DVD-R read speed 8 x
DVD-RW read speed 4 x
DVD-RW write speed 4 x
DVD+RW read speed 4 x
DVD+RW write speed 4 x
CD-R read speed 24 x
CD-R write speed 24 x
CD-RW read speed 24 x
CD-RW write speed 4 x
DVD drive compatibility CD-ROM, CD-R/RW, DVD-ROM, DVD+R/RW, DVD+-R (DL), DVD-RAM
Audio
Built-in microphone
Camera
Camera included
Networking
Internal modem
Bluetooth
Bluetooth is a low-power radio technology developed to replace the cables and wires currently used to link or connect electronic devices such as personal computers, printers, and a wide variety of handheld devices including mobile phones. Because it uses radio-wave connectivity, a Bluetooth-enabled device has a constant, established connection to whatever browser it uses. This saves the user the trouble of logging on to check for emails or news updates, for example.
Wireless technology WLAN (802.11b/g)
Modem speed 56 Kbit/s
Modem type V.90
Wireless network support 802.11b/g
Wireless compliancy Wi-Fi®
Networking speed
Network connectivity can be via Ethernet LAN (typically 10/100/1000 Mbps), Wireless LAN, or a traditional dial-up model (with separate fax and data speeds).
10/100 Mbps Base-TX
Networking topology Ethernet LAN
Operating system/software
Operating system provided Windows Vista Home Premium Edition
Certificates
Certification S.M.A.R.T.
Energy management
Battery technology Lithium-Ion
Battery life
Maximum battery life in hours. Mobile Mark™ (2002) is the standard often used to benchmark battery life time. In some cases battery life can be extended by adding extra batteries.
2.17 h
Number of battery cells 6 pcs
Connectivity
ExpressCard slot
VGA (D-Sub) ports quantity 1
Ethernet LAN (RJ-45) ports quantity 1
TV out port
Description of TV Out port
USB 2.0 ports quantity
USB 2.0 ports have a data transmission speed of 480 Mbps, and are backwards compatible with USB 1.1 ports. You can connect all kinds of peripheral devices to them.
3
Modem (RJ-11) ports 1
Speaker/ headphone/ line-out jack 1
Microphone, line-in jack
S/PDIF out port
DC-in jack
DVI port
Infrared data port
A data port that uses infra-red data association (irDA) as the standard for wireless communications between computer and mobile phone devices. For example, to update the phone list on your irDA-enabled PC, you would line up the infra-red ports on each device and then transfer the phone information to your PC. This is a wireless transfer, so you don't need a cable or extra software.
SmartCard slot
CardBus PCMCIA slot type
TV in port
Port replicator
Weight & dimensions
Weight
Weight of the product without packaging (nett weight). If possible, the nett weight is given including standard accessories and supplies. Please, note that sometimes the manufacturer is giving a too commercial interpretation of product weight, by leaving out the weight of accessories and/or supplies.
3180 g
Depth 292 mm
Width 398 mm
Height (front) 35 mm
Height (rear) 43 mm
Technical details
Type PC
Pointing device Touchpad
2 offers, from €535.54  

Product comments
johncena_2049
2008-12-31 21:07:09
what the hell we cannot even connect to the mobile phones via bluetooth in this machine this is a total waste of money are there other alternatives for bluetooth except cable connection to connect to the mobile phones
eric
2008-09-14 11:08:00
its agood machine BUT you must avail XP drivers for users.orelse we shall join dell who have already given xp driver that is the bullshit we want
eric
2008-09-14 11:07:27
its agood machine BUT you must avail XP drivers for users.orelse we shall join dell who have already given xp driver that is the bullshit we want
Show all comments>>

User comments
For product or price questions please contact the connected shops. For other questions contact our customer service.
Your email address
Comment
*Please, type the big numbers shown here into the box